AnsweredAssumed Answered

Code explanation

Question asked by birsan.paul on Nov 21, 2014
Latest reply on Nov 24, 2014 by birsan.paul
 Hi! 

 I would be glad if someone would explain the steps this code does in order to set up the AF9 on GPIOD for CAN pins. It is in a nice example, and I cannot figure it out why does the setting like this. 

void GPIO_PinAFConfig(GPIO_TypeDef* GPIOx, uint16_t GPIO_PinSource, uint8_t GPIO_AF)
{
  uint32_t temp = 0x00;
  uint32_t temp_2 = 0x00;
  
  /* Check the parameters */
  assert_param(IS_GPIO_ALL_PERIPH(GPIOx));
  assert_param(IS_GPIO_PIN_SOURCE(GPIO_PinSource));
  assert_param(IS_GPIO_AF(GPIO_AF));
  
  temp = ((uint32_t)(GPIO_AF) << ((uint32_t)((uint32_t)GPIO_PinSource & (uint32_t)0x07) * 4)) ;
  GPIOx->AFR[GPIO_PinSource >> 0x03] &= ~((uint32_t)0xF << ((uint32_t)((uint32_t)GPIO_PinSource & (uint32_t)0x07) * 4)) ;
  temp_2 = GPIOx->AFR[GPIO_PinSource >> 0x03] | temp;
  GPIOx->AFR[GPIO_PinSource >> 0x03] = temp_2;
}

Outcomes