AnsweredAssumed Answered

spbt2632c1A Bluetooth

Question asked by wint.angelina on Oct 8, 2014
Latest reply on Oct 8, 2014 by Clive One
Hello :),

I need help to solve the communication between processor C805 and BL module. Devices communicate via UART (serial port -> TX / RX pins) and I need to do a basic setup. Then send it AT commnads  BL module. UART is working well, and after turn on BL module get an answer
 
AT-AB -CommandMode-
AT-AB BDAddress BDR

But when I send some AT commands are unanswered.
I do not understand the syntax is respected .. just do not know whether statements end with \ r \ n or something like that. Or whether they are poorly chosen AT commands in the communication.

Please help me :) guys, tnx



Outcomes