AnsweredAssumed Answered

DMA2 (Can't Configure Seperate Streams for ADC1 and ADC2)

Question asked by Robin on Sep 18, 2014
Latest reply on Sep 19, 2014 by Clive One
I have the STM32F407 Discovery board.
I am configuring two streams using DMA and ADC
The first stream uses Stream 0 channel 0 of the DMA 2 ie ADC1 which reads the value of ADC chanel 9 1N9 and gets sent to circular buffer and send as audio 8Khz.
The second stream uses Stream 2 channel 1 of DMA2 ie ADC2 which reads values of ADC channels 2N - 0,1,5,6,7,8 at 1Khz. using DR and Tim3 TRGOut as the trigger.

If I configure each stream independently it works (ie I have not configured the other).
If I configure both DMA2/Streams/ADCX. The first configured DMA2_streamX_Interupt handler does not fire.

Outcomes