AnsweredAssumed Answered

STM32F429I-DISCO external SDRAM as data Memory

Question asked by mangraviti.giova.001 on Sep 10, 2014
Latest reply on Sep 10, 2014 by mangraviti.giova.001
Goodmorning,

I would like to use, on the STM32420Disco demo board, the external SDRAM as data memory.
The FMC example present on the STD lybrary is not taylored to work properly on the disco board, so I have imported the necessary functions to init the memory, the FMC and the relative I/O, from the FMC_SDRAM example dedicated for the disco board.
The problem is that as soon as I run the program from the main the micro is pushed into an fault_Hardware handler.
Can somebody help me?
Thanks

Outcomes