AnsweredAssumed Answered

STM32F4 Discovery USB Problem on REC and Playback Demo

Question asked by raj.rahul on Aug 23, 2014
Latest reply on Aug 23, 2014 by Clive One
Hi.
I have tried to build a project using the provided source code in Eclipse IDE. I could do simple live recording and play back from Internal Flash. But I got the following errors  when using USB for recording and playback(ST provided demo) .
../src/USB/usb_dcd.c:93:7: error: 'USB_OTG_CORE_HANDLE' has no member named 'dev'
   pdev->dev.device_status = USB_OTG_DEFAULT;
Can any one help me to fix these errors.

Outcomes