AnsweredAssumed Answered

Flash loader demonstrator not working. stm32f407-disc

Question asked by erjavec.klemen on Aug 1, 2014
Latest reply on Aug 2, 2014 by erjavec.klemen
Hello everybody

I am trying to disable read out protection (level 1) on my stm32f407-discovery with flash loader demo (v2.6).
I've connected Boot0 to Vdd, PB2 (boot1) to Gnd and my serial port (via max232) to usart1 PA9 and PA10. When I connect to PA9 led7 turns green.
The flash loader demo doesn't recognize my device. I've also tried with usart3 (led7 is turned off) but the result is the same.

Outcomes