AnsweredAssumed Answered

Raw readings from accelerometer in the LSM9DS0

Question asked by rasteiro.miguel on Feb 27, 2014
Latest reply on May 21, 2014 by winer.kris
Hi,

My raw readings from the accelerometer of the LSM9DS0 MEMS have a big offset in  two axis, it's about 0.15 G in the x-axis and .07 G in the z-axis. i find these offsets about 15% and 7% in these axis are a bit strange, especially when is said that the sensor come calibrated from factory. Could you confirm me if is a normal situation?

Regards 
Miguel Rasteiro

Outcomes