AnsweredAssumed Answered

Sequence of ADC conversion in Regular Simultaneous Mode

Question asked by Selva.Solo on Jun 18, 2014
Latest reply on Jun 25, 2014 by Clive One
Hi Everyone
     In my project, I need to capture 6 channel ADC signals in Regular Simultaneous Mode. for that, I just started for 2 channels (Channel 0 in ADC1 & Channel 1 in ADC2). Since it does simultaneous conversion, I gave the conversion sequence as 1,1 (i.e Rank for Ch0 is 1 & Ch1 is 1). It is working fine. But when i try it for 6 channels I'm getting problem, I'm not getting the actual signal, what I'm giving. I just confused with the sequence. For 6 channels i gave the sequence as (ADC1 Ch0 is 1 & ADC2 Ch1 is 1 ) (ADC1 Ch2 is 2 & ADC2 Ch3 is 2 ) (ADC1 Ch4 is 3 & ADC2 Ch5 is 3 ) is it right ???  can anyone help me... Please.

Part Number - STM32F103VDT7
Number of Samples - 256

Thank You...

Regards 
Selva
     

Outcomes