AnsweredAssumed Answered

EWARM St-Link debug of STM32F4 Discovery board not using .intvec

Question asked by phillips_jr..clyde on Jun 17, 2014
Latest reply on Jun 23, 2014 by phillips_jr..clyde
The PC is always pointing to 0x08000188 (after the .intvec allotment )

So as a workaround I put a B <label> there. The label value is incorrect.
This is not using the flash loader. If I use it it fails citing writes to the CCM area.

All the generic STM32F4 manual don't mention the 0x08000000 as even being in the memory map. And i can't set the intvec to flash load at 0x0.

Is there information about these issues anywhere?

Thanks Clyde

Outcomes