AnsweredAssumed Answered

SPI full duplex communication using software NSS for STM32F103ZE

Question asked by mukherjee.ayan on Jun 11, 2014
Latest reply on Jun 12, 2014 by yao.randy.001
Hello. I am trying to run SPI full duplex communication using software NSS for STM32F103ZE downloaded from STM32 peripheral example. Its compiling and downloading without error. I have connected GPIOA 5,6,7 (SPI1) with GPIOB 13,14,15 (SPI2) respectively.
The program is running ok till the while loop 'while (SPI_I2S_GetFlagStatus(SPIz, SPI_I2S_FLAG_RXNE) == RESET);' The program is not moving any further. It seems there is some problem with reception of data.
Please suggest a solution to the problem.
Thanks.

Outcomes