AnsweredAssumed Answered

Stepper motor (half step and micro step ) in stm32f030

Question asked by das.sanjib on Apr 16, 2014
Latest reply on Apr 21, 2014 by das.sanjib
Hi
I am writing a code to drive a stepper motor half step as well as micro step. Before going towards the code first the driver what I am using is H bridge.The fig shown below



A Winding1           B Winding 2
H Bridge               H Bridge
A0 | /A0                         B0 | /B0

A1 | /A1                        B1 | /B1

I am really a new guy in this and i have never drive a motor I have written code for half step but I am not sure it will work V supply is 5 volt and the motor is 2 volt . Delay or you can say acceleration for that I have used DMA. but I think I have to use pwm too for (got to know from internet source ) to control the heat of the motor how to use that in my code along with the present code . How to achieve for microstepping too .Please help me . I don't know how to do it . Any help will be really appreciated
 
Half step table (higher Pchannel, Lower N channel)
A0   A1   A0/   A1/  B0  B1  B0/  B1/
0       0     1      1      0     0    1     1
0       0     1      1      1     0    1     0
0       0     1      1      1     1    0     0
1       0     1      0      1     1    0     0
1       1     0      0      1     1    0     0
1       1     0      0      1     0    1     0
1       1     0      0      0     0    1     1
1       0     1      0      0     0    1     1

I have paste the code below which is done so far Please help

#include <stm32f0xx.h>
#include "stm32f0xx_adc.h"
#include "stm32f0xx_gpio.h"
#include "stm32f0xx_rcc.h"
#include "stm32f0xx_usart.h"
#include <stm32f0xx_syscfg.h>
#include "stm32f0xx_rcc.h"
#include "stm32f0xx_misc.h"
#include "stm32f0xx_tim.h"
#include "stm32f0xx_dma.h"



#include "stdio.h"

/*****************************************************************************************/
/**
 * global variables
 *
 */
int index = 0;

#define SAMPLES 4

uint32_t SampleVector[SAMPLES] = {60000 -1 , 60000 -1 , 60000 -1, 60000 -1}; // TIM2 32-bit   // 5 milli sec

/**************************************************************************************/

void RCC_Configuration(void)
{
  /* DMA1 (TIM2 on APB1) clock enable */
  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);

  /* TIM2 clock enable */
  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);

  /* GPIOA clock enable */
  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
}

/**************************************************************************************/

void GPIO_Configuration(void)
{
  GPIO_InitTypeDef GPIO_InitStructure;




          GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
          GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
          GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
          GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
          GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
          GPIO_Init(GPIOC, &GPIO_InitStructure);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; // PA1 TIM2_CH2
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_Init(GPIOA, &GPIO_InitStructure);

  /* Connect TIM2 pin  */
  GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_1); // PA1 TIM2_CH2


  /*
       * PA8 A0, PA9 A1, PA10 A0/, PA11 /A1 FET 4 pins of left driver controlling the motor
    */

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
   GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
   GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8|GPIO_Pin_9|GPIO_Pin_10|GPIO_Pin_11;
   GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
   GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
   GPIO_Init(GPIOA,&GPIO_InitStructure);

   /*
         *  PB4 B0, PB5 B1, PB0 B0/, PB1 /B1 FET 4 pins of right driver controlling the motor
      */
   GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
      GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
      GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_0|GPIO_Pin_1;
      GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
      GPIO_Init(GPIOB,&GPIO_InitStructure);

     /*
      * Configure ADC3 Channel12 pin as analog input
      */
          GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
          GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
          GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
          GPIO_Init(GPIOC, &GPIO_InitStructure);

}

/**************************************************************************************/

void DMA_Configuration(void)
{
  DMA_InitTypeDef DMA_InitStructure;

  DMA_DeInit(DMA1_Channel3);


  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&TIM2->ARR;
  DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&SampleVector[0];
  DMA_InitStructure.DMA_DIR =  DMA_DIR_PeripheralSRC;
  DMA_InitStructure.DMA_BufferSize = SAMPLES;
  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; // TIM2 is 32-bit
  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
//DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
  DMA_InitStructure.DMA_Priority = DMA_Priority_High;
  DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
//  DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable;
//  DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;
 // DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
//  DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

  DMA_Init( DMA1_Channel3, &DMA_InitStructure);

  DMA_Cmd(DMA1_Channel3, ENABLE);
}

/**************************************************************************************/

void TIM3_Configuration(void)
{
  TIM_TimeBaseInitTypeDef TIM_InitStruct;
  TIM_OCInitTypeDef TIM_OCInitStructure;

  /* Time base configuration */
  TIM_InitStruct.TIM_Prescaler = 4 - 1;                // This will configure the clock to 32 MHz
  TIM_InitStruct.TIM_CounterMode = TIM_CounterMode_Up; // Count-up timer mode
  TIM_InitStruct.TIM_Period = 60000 - 1;                 //  5ms initially
  TIM_InitStruct.TIM_ClockDivision = TIM_CKD_DIV1;     // Divide clock by 1
  TIM_InitStruct.TIM_RepetitionCounter = 0;            // Set to 0, not used
  TIM_TimeBaseInit(TIM3, &TIM_InitStruct);

  TIM_ARRPreloadConfig(TIM3, ENABLE);

  /* Output Compare Toggle Mode configuration: Channel2 - so we can actually measure widths */
  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; // 80 KHz
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
  TIM_OCInitStructure.TIM_Pulse = 1;
  TIM_OC2Init(TIM3, &TIM_OCInitStructure);

  /* TIM2 Update Interrupt enable - for whatever purpose, likely to saturate */
  TIM_ITConfig(TIM3, TIM_IT_Update, ENABLE);

  /* TIM2 Update DMA Request enable */
  TIM_DMACmd(TIM3, TIM_DMA_Update, ENABLE);

  /* TIM2 enable counter */
  TIM_Cmd(TIM3, ENABLE);
}

#if 0
void ADC_init()
{
    ADC_InitTypeDef ADC_InitStructure;
    ADC_CommonInitTypeDef  ADC_CommonInitStructure;
     RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3,ENABLE);
    /* ADC Common Init **********************************************************/
    ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
    ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
    ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
    ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
    ADC_CommonInit(&ADC_CommonInitStructure);


    /* ADC3 Init ****************************************************************/

    ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
    ADC_InitStructure.ADC_ScanConvMode = DISABLE;
    ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
    ADC_InitStructure.ADC_NbrOfConversion = 1;
    ADC_Init(ADC3, &ADC_InitStructure);
     ADC_Cmd(ADC3,ENABLE);

    /* ADC3 regular channel12 configuration *************************************/
    ADC_RegularChannelConfig(ADC3, ADC_Channel_12, 1, ADC_SampleTime_3Cycles);


    /* Enable DMA request after last transfer (Single-ADC mode) */
     ADC_DMARequestAfterLastTransferCmd(ADC3, ENABLE);




    ADC_AnalogWatchdogThresholdsConfig(ADC3, 2200, 0);
    ADC_AnalogWatchdogSingleChannelConfig(ADC3, ADC_Channel_12);
    ADC_ClearFlag(ADC3, ADC_FLAG_AWD);
    ADC_AnalogWatchdogCmd(ADC3, ADC_AnalogWatchdog_SingleRegEnable);
    ADC_ITConfig(ADC3, ADC_IT_AWD, ENABLE); // Enable ADC1 AWD interrupt




    NVIC_InitTypeDef NVIC_InitStructure;


    /* Configure and enable ADC interrupt */
    NVIC_InitStructure.NVIC_IRQChannel = ADC_IRQn;
    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
    NVIC_Init(&NVIC_InitStructure);
     ADC_SoftwareStartConv(ADC3);
}
#endif
/**************************************************************************************/

void NVIC_Configuration(void)
{
  NVIC_InitTypeDef NVIC_InitStructure;

  /* Enable TIM2 Interrupt */
  NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPriority = 0;
  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
  NVIC_Init(&NVIC_InitStructure);

}

/**************************************************************************************/

void TIM3_IRQHandler(void)
{
#if 0
    static int i = 0;
  if (TIM_GetITStatus(TIM3, TIM_IT_Update) != RESET)
  {

      if (i == 0)
      {
          GPIO_SetBits(GPIOC, (GPIO_Pin_8 | GPIO_Pin_9));
          i = 1;
      }

      else
      {

          GPIO_ResetBits(GPIOC, (GPIO_Pin_8 | GPIO_Pin_9));
         i = 0;
    }
    TIM_ClearITPendingBit(TIM3, TIM_IT_Update);

  }
#endif
#if 1
  if (TIM_GetITStatus(TIM3, TIM_IT_Update) != RESET)
  {
      switch(index)
         {
         case 0:
        // GPIO_Write(GPIOA,GPIO_Pin_8|GPIO_Pin_11);
             GPIOA->ODR &= 0xF0FF;
             GPIOB->ODR &= 0xFFCC;
             GPIOA->ODR |= 0x0C00;
             GPIOB->ODR |= 0x0003;
             break;

         case 1:

        // GPIO_ResetBits(GPIOB,GPIO_Pin_4|GPIO_Pin_1 );


          GPIOB->ODR &= 0xFFCC;
          GPIOB->ODR |= 0x0011;
          //index = -1;
       // TIM_ITConfig(TIM3, TIM_IT_Update, DISABLE);
         break;

         case 2 :
             //GPIO_Write(GPIOB,GPIO_Pin_5|GPIO_Pin_0);

            GPIOB->ODR &= 0xFFCC;
             GPIOB->ODR |= 0x0030;
              TIM_ITConfig(TIM3, TIM_IT_Update, DISABLE);
         break;

         case 3:
             // GPIO_ResetBits(GPIOA,GPIO_Pin_8|GPIO_Pin_11);
             GPIOA->ODR &= 0xF0FF;
             GPIOA->ODR |= 0x0500;

         break;

         case 4:
             //GPIO_Write(GPIOA,GPIO_Pin_9|GPIO_Pin_10);
             GPIOA->ODR &= 0xF0FF;
             GPIOA->ODR |= 0x0300;

         break;

         case 5:
         //    GPIO_ResetBits(GPIOB,GPIO_Pin_5|GPIO_Pin_0);
             GPIOB->ODR &= 0xFFCC;
             GPIOB->ODR |= 0x0011;
         break;
         case 6:
             // GPIO_Write(GPIOB,GPIO_Pin_4|GPIO_Pin_1);
             GPIOB->ODR &=  0xFFCC;;
             GPIOB->ODR |= 0x0003;
         break;
         case 7:
             //GPIO_ResetBits(GPIOA,GPIO_Pin_9|GPIO_Pin_10);
            GPIOA->ODR &= 0xF0FF;
             GPIOA->ODR |= 0x0500;
             index = -1;


         break;


         }
         index ++ ;
     // index = 0;
         TIM_ClearITPendingBit(TIM3, TIM_IT_Update);

  }
#endif
}


/**************************************************************************************/

int main(void)
{
  RCC_Configuration();

  NVIC_Configuration();

  GPIO_Configuration();

  //STM_EVAL_LEDInit(LED3);

  DMA_Configuration();

  TIM3_Configuration();

  while(1); // Don't want to exit
}

/**************************************************************************************/

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *   where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t* file, uint32_t line)
{
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

  /* Infinite loop */
  while (1)
  {
  }
}
#endif

/**************************************************************************************/

Outcomes