AnsweredAssumed Answered

STM32F439I-EVAL2 board support and configuring STM32CubeMX

Question asked by aiyer.kartik on Apr 15, 2014
Latest reply on Apr 15, 2014 by Clive One
I just purchased the STM32F439I-EVAL2. The board didn't come with any BSP or code that I can build in IAR. I'm guessing I need to use STM32CubeMX to configure the Bsp and setup the pinouts used on the board. Unfortunately this is fairly complicated and I would like some support on getting the bsp for this specific evaluation board. If there is a .ioc file for the evaluation board, that would be great, otherwise I would appreciate some support in setting up STM32CubeMX to generate the required code and libraries I want to use for my design.

Thanks
Kartik

Outcomes