AnsweredAssumed Answered

System Workbench Project Structure Question

Question asked by carbone.fabio on Nov 23, 2016
Latest reply on Nov 29, 2016 by FTITI.Walid

Hi, I have a question about the using of System Workbench and projects.

When I download a firmware from ST website, usually I put the extracted folder in the System Workbench workspace, then click Import -> Existing Project Into Workspace (copy project into workspace uncheked).

It works well, but I obtain a project with relative path and liked resource, I mean that the structure of the files that I can see from Eclipse is not the real structure of the files of the folder project. I don't like it, and it confuse me. 
If I want to obtain a "normal" structure, I usually copy/paste manually all file in order to recreate the original structure, then I insert include path and symbol. But it is hard and some time leads to compiling errors.

There is a way to do it automatically and safely?

Outcomes