AnsweredAssumed Answered

problem with LSM330dlc

Question asked by incicco.sebastian on Feb 13, 2014
Hi, i have a problem with LSM330dlc. 
Sometimes the gyroscope doesn't work fine. The gyroscope sends measures constants and then I should to disconnect the sensor of VCC (reset).
After, in most cases it works well.
With the accelerometer i don't have any problem.
My code is (SPI communication):
-------
WriteSpiGiro(0x20,0xFF);     // CTRL_REG1_G. Power ON: 760Hz; Cut-Off: 100Hz; X,y,Z axis: On
WriteSpiGiro(0x21,0x20);  
WriteSpiGiro(0x23,0x10);
-------

the other register are by default.
is this particular sensor my problem? has this problem happened to someone else? 

thanks

Outcomes