AnsweredAssumed Answered

STM32L0Cube UART HAL pulls in extraneous floating point code

Question asked by kao.tony.001 on Oct 30, 2016
Latest reply on Dec 14, 2016 by Anders Dam Kofoed
Hi,

The latest STM32L0Cube UART Hal pulls in unnecessary floating point code when initializing the UART. The culprit is the __DIV_LPUART macro, which contains a floating point number (256.0). When replaced with the version from STM32L4Cube, it no longer pulls in floating point libraries.

The extra code takes up at least 6KB of extra code space, which is a lot for the smaller L0's.

Tony

Outcomes