AnsweredAssumed Answered

STM32Cube doesn't copy 'Drivers' files in project

Question asked by Masriera.Jordi on Oct 28, 2016
Latest reply on Nov 3, 2016 by Masriera.Jordi
Hi.

I've generated a project using Cube, but the Drivers directory is void (it has subdirectories but any file), and then the project is full of errors.

I've attached the project. The project properties are:
- STM32F769I-DISCO board
- Enable SD 4 bit wide bus
And the generate it. (I know it has a clock error).

Cube version 4.17.0
STM32Cube v1.0
STM32Cube_FW_F7 V1.5.1

If i select FW package STM32Cube_FW_F7 V1.5.0 then it copies all the files.

Is this a bug or I'm doing/I have something wrong?

Attachments

Outcomes