AnsweredAssumed Answered

changing microcontroller type in STM32CubeMX

Question asked by Danielyan.Varuzhan on Oct 21, 2016
Latest reply on Oct 21, 2016 by ForumSTM32.ForumSTM3
Is it possible to change in the STM32CubeMX project the microcontroller type, keeping  all
settings: pinout, etc.?
For example, I have a proven project for the STM32F746 (single precision floating), which I
need to change for the F767 (double precision), without affecting all other settings?
If not, then it is very desired feature for the next versions of the STM32CubeMX.

Great thanks, 

Varuzhan

Outcomes