AnsweredAssumed Answered

STM32CubeMX together with KEIL mdk 5

Question asked by Mark de Groot on Sep 30, 2016
Latest reply on Oct 6, 2016 by STM32Cube-T
Hello,

I have problems using STM32CubeMX together with KEIL mdk 5.

When starting a new project in Keil I can use all the Keil functionality, but when I open Cube from the project runtime environment and initialize everything in there, than I am not able to include Middlewares from Cube in my project. It doesn't include all the files as it does when starting a project in Cube. I can add them manually and this works ok, but this isn't a very maintenance friendly way of coding.

On the other hand, when starting a project in Cube I can't add all the Keil CMSIS and Board Support(stm32f4) functionality(only adding RTOS RTX is doable) without getting low level errors.

Is there a way of using those two together and use all of there functionality on a user-friendly way?


I hope someone can help me with this issue.
(and this post is placed instead of having to type it all over..)

Outcomes