AnsweredAssumed Answered

STM32 Cube MX bootloaded application

Question asked by boyd.bruce on Sep 27, 2016
Latest reply on Sep 27, 2016 by FTITI.Walid
Does anyone know if it is possible to get STM32 CubeMX to generate a project that is "predefined" to be loaded using a bootloader?

Essentially, this would involve being able to specify the program load address and vector table offset. The obvious place for this would be in the linker settings portion of the Project Settings dialog, along with the specification of the heap and stack size.

Failing that, does anyone know if there is already a way to achieve the same result using Cube? 

Thanks,

Outcomes