AnsweredAssumed Answered

Change static library target device in SW4STM32

Question asked by heifets.gregory on Sep 11, 2016
Latest reply on Sep 22, 2016 by FTITI.Walid
Hi,


I use the SW4STM32 IDE and would like to create a generic static library.
When I go to New Project tab and select static library in "Project type", I can create "Ac6 STM32 MCU GCC" or "Cross GCC" project.


Naturally I go to the Ac6 project and then I have to select  the target MCU. 
The problem begins, when I want to change the target MCU. There is a warning not to do that, and even if I try to change the target in the settings, the target won't change.
The advice is to create a new project, but that would be difficult if I want to use the library on many projects.


I think I could create GCC project by referencing the toolchain and everything else, but it looks like an inefficient way.


I would like to ask if there a good way to change library target device?

Outcomes