AnsweredAssumed Answered

STM32F334 SPI

Question asked by B_U.Vishal on Aug 29, 2016
Latest reply on Jul 13, 2017 by Stef Nah
Hi! I am new to STM32 microcontrollers and SPI. I'm currently working on STM32F334R8T6 (Nucleo board 64-pin package) and need to configure it as spi full duplex master without crc for operating MAX31865 temperature sensor. I'm also confused about NSS. The chip select is high in idle state. Using the STM32Cube for configuring
Can I plz get an SPI sample code for this microcontroller either in polling or interrupt mode??

Outcomes