AnsweredAssumed Answered

X-Cube-Crypto Library CubeMX Help

Question asked by yarema.andriy on Aug 9, 2016
Latest reply on May 10, 2018 by Damien Sauveron
I downloaded X-Cube-Crypto Library from the email and i have the zip. Issue is that i cant seem to find anything that would install it into the CubeMX software. I can browse the zip and see the files and examples included but when i try to install new libraries on CubeMX from local it says "This Package version is not managed on this version of STM32CubeMX".

My version is 4.16.0 for CubeMX.

Is there a way to install this lib so that CubeMX is able to create the necessary C source files when project is generated?

Question 2 is about the fact that System Workbench is missing from the examples, and support for the F7 series. Is there a plan to add that anytime soon?

Thanks
Andriy

Outcomes