AnsweredAssumed Answered

External interrupts question

Question asked by obid.matic on Aug 7, 2016
Latest reply on Aug 17, 2016 by pribyl.adam
Hi.

Currently I use PA15 pin as external interrupt. The ISR routine is common for lines 10 through 15 and it is called EXTI15_10_IRQHandler. Now, I would like to have another signal connected to pin PB12, which has same IRQ Handler as PA15, and enable interrupt also for PB12. But I don't want to come into ISR when event on PB12 occurs. I just want to poll for the flag in EXTI->PR register. Interrupt (ISR) should occur only at event on PA15.

Is this possible or should I move one signal to different pin?

Thanks

Outcomes