AnsweredAssumed Answered

Error in STM32F4 V1.7.1 Std Periph Lib

Question asked by gin.adrian on Jul 28, 2016
Latest reply on Jul 28, 2016 by FTITI.Walid
In the file

stm32f4xx.h
<br>#define  DBGMCU_APB1_FZ_DBG_TIM1_STOP        ((uint32_t)0x00000001)<br>#define  DBGMCU_APB1_FZ_DBG_TIM8_STOP        ((uint32_t)0x00000002)<br>#define  DBGMCU_APB1_FZ_DBG_TIM9_STOP        ((uint32_t)0x00010000)<br>#define  DBGMCU_APB1_FZ_DBG_TIM10_STOP       ((uint32_t)0x00020000)<br>#define  DBGMCU_APB1_FZ_DBG_TIM11_STOP       ((uint32_t)0x00040000)

There are wrong, and should be APB2 instead of APB1, can we have this fixed up in the next release?

Outcomes