AnsweredAssumed Answered

TIM_OCMODE_PWM1 not selectable in STM32CubeMX

Question asked by michaeL on Jul 27, 2016
Latest reply on Jul 28, 2016 by michaeL

Hi there,

I just want to generate a simple Pulse Width Modulation with the STM32F303RE with Timer 1 / Output Compare Channel 3.

But I can not select the desired mode TIM_OCMODE_PWM1 for sConfigOC.OCMode.

Do I have to configure something else that it is available or is it an issue of the STM32CubeMX  4.16.0 tool?

I have installed STM32CubeF3 Firmware Package V1.6.0 / 01-July-2016 .

The drop down menu looks like in the attachment.

Best regards,

michaeL

Outcomes