AnsweredAssumed Answered

A CUBE issue: float mode from hard to "soft" with no explanation

Question asked by ELBY on Jul 7, 2016
Latest reply on Jul 8, 2016 by ELBY
Hi,

i have a problem with CUBE and System Workbench.

Each time i click the "Generate code" the FPU mode in Drivers and/or Middlewares is randomly switched from hard to soft (--abi-float=soft)

The code won't compile then.

It's very annoying because this behavior is very random: sometimes only the Drivers branch is touched, sometimes both Drivers and Middlewares are changed.


Is my problem unique or there's a solution for a "permanent" float setting in Eclipse?
I need "hard".

-
Using the System Workshop Luna Release 2 (4.4.2) and Cube MX 4.14.0 on Windows.

Outcomes