AnsweredAssumed Answered

CubeMX Bug Report: Missing HCD_SPEED_HIGH option

Question asked by todor.todorov on Jul 2, 2016
Latest reply on Oct 7, 2016 by STM32Cube-T
Hello,

I have a project using the STM32F429 MCU with USB_OTG_HS, USB_HOST, and FatFs enabled. When configuring the  USB_HS peripheral in the Configuration tab, the CubeMX tool offers only Low and Full Speed as setting options - see attached screenshot. But according to UM1720 "STM32Cube USB host library" manual, section 6.4.3 (page 41), hhcd.Init.speed can be one of HCD_SPEED_FULL or HCD_SPEED_HIGH.

Comments?

Thanks for your attention.

Best regards,

T. Todorov

Attachments

Outcomes