AnsweredAssumed Answered

Need help with ADC using MCBSTM32F400 Evaluation Board

Question asked by guru on Jun 29, 2016
Latest reply on Jun 29, 2016 by FTITI.Walid
Hi friends,

I need a help. If possible someone please help me.

I'm using Keil MCBSTM32F400 Evaluation board. and I have stm32cubemx v4.15 also. I'm having circuit which gives me some voltage between 0 to 5V which will be changing frequently. I need to change the voltage to a digital value using adc every 100ms and display the value in the LCD screen which is there is the evaluation board. 

This is my requirement. I was working with 8 bit microcontrollers previously. So understanding this is little bit difficult for me. if anyone could attach an .ioc file, it would be really useful. 

Outcomes