AnsweredAssumed Answered

Pin configuration in cubemx broken ?

Question asked by brown.geoffrey.001 on Jun 25, 2016
Latest reply on Jun 29, 2016 by Nesrine M
I'm using 4.14 (although I had the same behavior with the most recent build on a different machine) under OS X

When configuring the USB devices on an stm32f303VEx,  the pins are not correctly configured -- indeed there is no configuration for these pins generated.  Furthermore, the only thing I seem to be able configure through the user interface is the user label.  

This is true within the pin configuration window as described in the user manual.  For example, under the USB device configuration, selecting the pins only allows the user label to be changed.

This is both unexpected and annoying behavior -- is there some mechanism I am missing ?

Outcomes