AnsweredAssumed Answered

HTTP Server. Webpage in SD

Question asked by llona.martin on Dec 13, 2013
Latest reply on Oct 12, 2014 by Pankaj
Hi Everyone,

I have a STM32F4Discovery board and I have implemented on it an http server using the lwip v1.41 stack. I also have implemented a micro-SD with SDIO and FATFS, and USB FS as a mass storage device. All of this is working fine together.

My question is if I can store the webpages in the SD card in binary format instead of using the fsdata.c inside the microcontroller flash. If so, how can I do that? Is there any example?

Thanks

Outcomes