AnsweredAssumed Answered

is there an ST-LINK V2 with the V2-A version firmware?

Question asked by Vermaak.Dirk on Jun 22, 2016
Latest reply on Jun 22, 2016 by ForumSTM32.ForumSTM3
Hi,

Does anyone know if there is an ST-Link (the actual small white unit) that runs the V2-A firmware that allows the  Mass storage option? 

I have an STM32F407G-DISC1 with this feature (with ST-LINK/V2-A only) and it's great. However I have a custom board coming back and now need to use the external unit.

It is possible to upgrade the firmware in the ST-Link?

Many Thanks,

Dirk Vermaak

Outcomes