AnsweredAssumed Answered

STM32F3Discovery - can I upgrade the ST-LINK to V2-1 to have Virtual Com?

Question asked by Bogdan Golab on Jun 14, 2016
Latest reply on Jul 3, 2016 by Bogdan Golab
Hi,
I noticed that STM32F3 has PC4 and PC5 connected to ST-LINK USART (or at least a bridge needs to be soldered).

I wonder if I can upgrade the standard F3Discovery firmware (V2) to version V2-1 which support Virtual Com.

I like VCOM feature which is available by default on nucleo boards running V2-1 ST-link firmware.

Thanks,
Bogdan

Outcomes