AnsweredAssumed Answered

HTTP server from cube firmware?

Question asked by Turboman on Jun 7, 2016
Latest reply on Jun 13, 2016 by Turboman
Hi,
   are there any tutorials for getting an HTTP server working from cube firmware?

I found the demo project in the F7 cube firmware V1.4.0 which displays which tasks are running on FreeRTOS. Works fine, great. Now I want to modify that, but it's a project with referenced files.

I would like:
Fatfs (on SD card)
LwIP http server
http server running from files on the sd card.
LCD status display on STM32F746 disco board.

Is there an easy way to make the above? CubeMX doesn't seem to do the BSP side of things properly, and SW4STM32 doesn't seem to do the LwIP side of things correctly, it just includes everything; I've just been tracking down broken include dependencies for the past day.

How have other people done this? 

Outcomes