AnsweredAssumed Answered

cubeMX bug:Import STM32F769 project into SW4STM32

Question asked by wu.albert.002 on Jun 3, 2016
Latest reply on Jun 6, 2016 by ForumSTM32.ForumSTM3
When import an STM32CubeMX generated project under System Workbench for STM32 follow the instruction of openstm32.org. Numerous errors shown:

unknown type name 'GPIO_TypeDef'
'GPIOC' undeclared (first use in this function)

and so on.

In order to solve this problem, a macro definition
#define STM32F769XX
should be added
manually

Meanwhile, the STM32F769NIHx_FLASH.ld can't be complied because their is a error in line 55
_estack = %stack%;    /* end of RAM */

it should be replaced to
_estack = 0x20080000;    /* end of RAM */
then the project can complies well.

Outcomes