AnsweredAssumed Answered

lwIP and SYS_LIGHTWEIGHT_PROT

Question asked by Spencer Oliver on May 27, 2016
Hi,

Just been testing some software that uses the STM32CubeF4 version of lwIP 1.4.1 stack.
With asserts enabled we were very occasionally seeing one triggered in pbuf.c:950.

LWIP_ASSERT("pbuf_free: p->ref > 0", p->ref > 0);

For info this part of code is enclosed in a SYS_ARCH_PROTECT/SYS_ARCH_UNPROTECT block, but as SYS_LIGHTWEIGHT_PROT was 0 it was not protected.

Looking into the lwIP docs I see that when using an OS/interrupts you should really define SYS_LIGHTWEIGHT_PROT to 1 so that the relevant block is protected.

If I define SYS_LIGHTWEIGHT_PROT to 1 in our code we see no more asserts.

A quick grep of ST sample code and I see that SYS_LIGHTWEIGHT_PROT is always 0. Is this really correct ?

Did a quick check of an older project that used another vendor Cortex-M3 product and they actually checked that SYS_LIGHTWEIGHT_PROT was 1 in the driver code.

Regards

Outcomes