AnsweredAssumed Answered

STM32CubeMx - STM32Cube - MEMS1 confusion

Question asked by katzenberger.michael on May 5, 2016
Latest reply on Jan 28, 2017 by Bogdan Golab
Hi !

I'm totally lost how to use these tool to setup a own project because I don't figure out how these tool are interacting.

For example I like to use the NUCLEO-F411RE board with X-NUCLEO-IKS01A1 expansion board.

I've installed STM32CubeMx including STM32CubeF4 Firmware Package V1.11.0 to support the NUCLEO-F411RE board.
To use X-NUCLEO-IKS01A1 I've installed STM32CubeExpansion_MEMS1_V2.1.0 but obviously this SW package can't be integrated in STM32CubeMx.

The question is now how to "merge" the STM32CubeMx generated files with the MEMS1 driver / BSP files (in an easy and convenience manner).

Thanks !

Michael.

Outcomes