AnsweredAssumed Answered

BSP functions in CubeMX

Question asked by aa.andrea on May 3, 2016
Latest reply on May 7, 2016 by aa.andrea
Hi,
I'm using CubeMX and System Workbench by AC6 on STM32F407-vgt6 to develop some basic projects for university purposes. First of all I'm studying Cube firmware's examples to understand how to work with the board in the right way and I noticed the use of some functions such as "BSP_LED_On(LED4);" that are not defined in the HAL library, but in the BSP files.
When I try to generate a new CubeMX project and import it into eclipse, I can't see the BSP folder within the Driver folder which contains all the HAL and CMSIS drivers.
Is there a way to make CubeMX add this library in my project, too? Or, since I know where this file are saved, how to add it to the current project without build errors by Eclipse?

Thank you in advance.
A.A.

Outcomes