AnsweredAssumed Answered

STM32F427 SPI HAL MXCube

Question asked by White.John on Apr 21, 2016
Latest reply on Apr 25, 2016 by White.John
Hi,
I believe I have a problem with SPI bus.
I have set the SPI bus to set up and receive data from a ADC.
First off I have configured IO Pins to Clock Data from the ADC using PA5 - SClk, PA6 as MISO and PA7 as MOSI and works fine for all 8 channels albeit slow.

I have reconfigured using MX Cube to configure the SPI bus.
The code fragment is as below:-

              // Code to wait for D_Ready;


              Set_CS(P_LOW);   // Set CS low on ADC

                                               
HAL_StatusTypeDef status = HAL_SPI_Receive(&hspi1, SPI1_Data_Read_ADC1, 4, 1000);  
                                                        
               if(status != HAL_OK) { return status; };                                             
                                             
                                                
                                                        
           Set_CS(P_HIGH);   // Set ADC CS High

This runs OK with Receive set to 4 bytes if I incease to 5 bytes the SPI stops clocking, I have an Oscilloscope(pico) on the Data, Clock and D_Ready and CS and all seems normal with 4 bytes but the SClk stop with 5 bytes +.
Changing CPOL, Edge and Baud rate has no effect.
Any help would be appreciated.  Thanks John W
 

Outcomes