AnsweredAssumed Answered

STM32F4Discovery + AD7680 via SPI

Question asked by oeztuerk.tugrul on Oct 7, 2013
Latest reply on Oct 9, 2013 by oeztuerk.tugrul
Dear community users,

at the moment I try to read the samples of the ADC AD7680 via SPI with the STM32F4 Discovery Board, but I did not get it to work.... Sadly, I don't have an oscilloscope or a logic analyzer to check the clocks etc...
Here is the connection information:
SDATA  on PC2
SCK       on PB10
CS          on PA3
MOSI is not connected, because I only read data from the AD7680.

Here is my code:


#include "stm32f4xx.h"
#include "stm32f4xx_dma.h"
#include "stm32f4xx_rcc.h"
#include "stm32f4xx_spi.h"
#include "stm32f4xx_gpio.h"
#include "misc.h"

/* Prototypes */
void SPIConfig(void);
void GPIOConfig(void);
void EnableRCC(void);


void Delay(__IO uint32_t nCount);

/* Defines */
#define SCLK        GPIO_Pin_10        
#define CS        GPIO_Pin_3        
#define SDATA        GPIO_Pin_2        
#define MOSI        GPIO_Pin_3        


#define LED_Green     GPIO_Pin_12
#define LED_Orange     GPIO_Pin_13
#define LED_Red     GPIO_Pin_14
#define LED_Blue     GPIO_Pin_15



int main(void)
{
    int i=0;

    uint8_t byte1 =1;
    uint8_t byte2 =1;
    uint8_t byte3 =1;

    unsigned int sample=1111;


    SystemInit();                    
    EnableRCC();                    
    GPIOConfig();                    
    SPIConfig();

    GPIO_SetBits(GPIOD,LED_Green);            

    /*GPIO_ResetBits(GPIOA,CS);
    Delay(1000000L);

    //SPI2->DR = 0;
    while(!(SPI2->SR & SPI_I2S_FLAG_RXNE));
    byte1=SPI2->DR;
    //SPI2->DR = 0;
    while(!(SPI2->SR & SPI_I2S_FLAG_RXNE));
    byte2=SPI2->DR;
    //SPI2->DR = 0;
    while(!(SPI2->SR & SPI_I2S_FLAG_RXNE));
    byte3=SPI2->DR;
    GPIO_SetBits(GPIOA,CS);

    sample = (byte1 << 11) | (byte2 << 3 ) | (byte3 >> 5 );*/

    while(1)
    {

        i++;

        GPIO_ResetBits(GPIOA,CS);
        Delay(1L);

        SPI2->DR = 0;
        while(!(SPI2->SR & SPI_I2S_FLAG_RXNE));
        byte1=SPI2->DR;
        SPI2->DR = 0;
        while(!(SPI2->SR & SPI_I2S_FLAG_RXNE));
        byte2=SPI2->DR;
        SPI2->DR = 0;
        while(!(SPI2->SR & SPI_I2S_FLAG_RXNE));
        byte3=SPI2->DR;
        GPIO_SetBits(GPIOA,CS);
        sample = (byte1 << 11) | (byte2 << 3 ) | (byte3 >> 5 );
    }


}


void Delay(__IO uint32_t nCount) {
  while(nCount--) {
  }
}

void SPIConfig(void)
{

    SPI_InitTypeDef SPI_InitStructure;

    SPI_InitStructure.SPI_Direction = SPI_Direction_1Line_Rx;            
    SPI_InitStructure.SPI_Mode = SPI_Mode_Master;                         
    SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;                    
    SPI_InitStructure.SPI_DataSize = SPI_FirstBit_MSB;                    
    SPI_InitStructure.SPI_BaudRatePrescaler=SPI_BaudRatePrescaler_32;    /* SCLK=42MHz/64=656.2kHz APB1=42 MHz, SYSCLK=168 MHz */
    SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;                /* CPOL=1 */
    SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;            /* CPHA=1 */
    SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;                            
    SPI_InitStructure.SPI_CRCPolynomial = 0;                            

    SPI_Init(SPI2, &SPI_InitStructure);                                    
    //SPI_SSOutputCmd(SPI2, ENABLE);
    //SPI_I2S_ITConfig(SPI2, SPI_I2S_IT_RXNE, ENABLE);
    SPI_Cmd(SPI2,ENABLE);                                                
    GPIO_SetBits(GPIOA,CS);


}


void GPIOConfig(void)
{
    GPIO_InitTypeDef GPIOLEDs_InitStructure;
    GPIO_InitTypeDef GPIO_InitStructure;

    /* Grüne und Blaue LED liegen auf PD12 und PD15 */
    GPIOLEDs_InitStructure.GPIO_Pin = LED_Green | LED_Blue;
    GPIOLEDs_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIOLEDs_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIOLEDs_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIOLEDs_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
    GPIO_Init(GPIOD, &GPIOLEDs_InitStructure);
    /* ------------------------------------------------------ */

    /* SCK Leitung liegt auf PB10 (SPI2) */
    GPIO_InitStructure.GPIO_Pin = SCLK;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOB, &GPIO_InitStructure);
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_SPI2);
    /* ------------------------------------------------------ */

    /* SDATA und MOSI Leitung liegt auf PC2 und PC3 (SPI2) */
    GPIO_InitStructure.GPIO_Pin = SDATA | MOSI;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    GPIO_PinAFConfig(GPIOC, GPIO_PinSource2, GPIO_AF_SPI2);
    GPIO_PinAFConfig(GPIOC, GPIO_PinSource3, GPIO_AF_SPI2);
    /* ------------------------------------------------------ */

    /* Chip Select liegt auf PA3 */
    GPIO_InitStructure.GPIO_Pin = CS;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* ------------------------------------------------------ */

}


void EnableRCC(void)
{
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);        
}

The datasheet of the AD7680 can be found here:
http://www.analog.com/static/imported-files/data_sheets/AD7680.pdf

Thank you in advance for any help !



Outcomes