AnsweredAssumed Answered

2 Cameras and an SD card

Question asked by luke.jorden on Sep 19, 2013
Latest reply on Sep 19, 2013 by Clive One
I am trying to develop a board that would use the STM32F407VGT6. I want to use the discovery board to mock it up. I am wondering if anyone knows if I can map 2 cameras and an SD card to the board. I only plan on using one camera at a time interfacing with the SD card I just noticed on the pin out for this particular chip it looked like it may be near impossible could some one give me some feed back as to away I am maybe over looking. As of now my idea was to flip form the alternate functions for of one set of pins that interface with the DCMI another for the cameras. Then Have the SDIO mapped to another set. But so far that looks bleak. Thanks

Outcomes