AnsweredAssumed Answered

STM32F0 Discovery - how to connect LCD display

Question asked by brak.martin on Sep 19, 2013
Latest reply on Sep 19, 2013 by Clive One
Hello everyone,


I have a problem with connecting STM32F0 Discovery board with Hantronix HDM16416H LCD display. I don't know which STM32 pins should be chosen to connecting STM and Hantronix LCD 4x20 display properly.


I have it set, as below:


LCD pin  -> STM pin:
E pin ->    PC10 pin
R/W pin -> PC11 pin 
RS pin -> PC12 pin
VDD pin -> 5V pin
D0 pin  ->  PA3 pin
D1 pin ->  PA2 pin
D2 pin -> PB12
D3 pin -> PB11
D4 pin -> PA7
D5 pin -> PB9
D6 pin -> PB8
D7 pin -> PA6


Is it correct?


There is a description of LCD from the manual.

270x.png

Attachments

Outcomes