AnsweredAssumed Answered

STM32L Possibility of timer expiry missing

Question asked by p.raul on Mar 25, 2016
Latest reply on Mar 28, 2016 by Clive One
I have Timer1(TIM1) channels configured @ different frequencies.I have loaded appropriate values inside the uhCCRX_Val register as well.The frequencies for channel 1,2 and 4 are 10,100 and 1 Hz , that means i must get the timer expiry at 100,10 and 1000 ms respectively.Since they are multiple of each other , is there a possibility of missing the timer expiries for any one.
for example
T1--channel1-->100ms,
T1--channel2-->10ms,
T1--channel4-->1000ms,

so at 1000ms I will get the expiries for channel 2 as well 4 after 10 and 100th time respectively besides for channel4 after 1th time.Is there any possibility that I may miss the expiries for any oneof them or all three expiries are bound to be captured.

 

Outcomes