AnsweredAssumed Answered

STM32F4-Discovery, DCMI interface, camera module OV5642

Question asked by hosS on Sep 3, 2013
Latest reply on Apr 23, 2014 by Clive One
Hi,
I'am starting a new project and I will need to interface the STM32F4 discovery with a camera module (OV5642) via DCMI interface. (I won't use an LCD module).
I will need a high resolution photo (>1024 pixel). I'am not sure if this is possible with the STM32F4.
I wanted to know if this is possible and if it is not what should I add as electronics to make it?

Outcomes