AnsweredAssumed Answered

Tracing Using ST-Link V2 and Ac6 System Workbench

Question asked by Stephen on Mar 21, 2016
Latest reply on Mar 21, 2016 by Clive One
The processor is an STM32F373VCT. The emulator probe is an ST-Link V2 iso.

I have on the board JTAG connections to all five of the processor's trace pins (CK, D0-D3). In the Ac6 System Workbench's Trace Control window I see that when I have a debug session in progress there is the message  "Tracing is not supported." Is this because the DBGMCU->CR register is left in its default state? If I set TRACE_IOEN, and TRACE_MODE bits in this register would tracing be supported? Or is tracing not supported in ST-Link V2 hardware?
 

Outcomes