AnsweredAssumed Answered

EVALKITST7580-1 works well in one direction and bad in other

Question asked by mazok.ilya on Mar 25, 2014

I have two EVALKITST7580-1.
One of them I configured as the master (call it device1). The other as the slave (call it device2).

When I run a ping gui, master sends 100 and receives 100 messages.

When I make device1 as slave and the device2 as master, master sends 100 and receives 82-92 messages.

Then I change the device places.

Again one of them I configured as the master (device2). The other as the slave (device1).

Master sends 100 and receives 100 messages. And when I make device2 as slave and the device1 as master, master sends 100 and receives 82-92 messages.

Again the problem with the transmission in one direction (from one corner of the room to the other, regardless of the device and its roles).

What happens? If this noise, they should interfere in both directions?

Outcomes