AnsweredAssumed Answered

Cannot boot from CAN

Question asked by pirot.john on Jun 28, 2013
Latest reply on Jul 10, 2013 by Giovanni Di Sirio

Hi,

I have the following setup. I'm using the SPC5604 at 8MHz, FAB and ABS pins are set to boot from CAN. A dedicated CAN probe is used from a PC to perform the CAN boot protocol. According to ST's application notes and datasheets I must sent my messages at 200kbds.

 

First I send the default password 0xFEEDFACECAFEBEEF to CANID 0x011 and according to the application note I shall receive an echo of this message at CANID 0x001. Unfortunately I do not receive any messages. Then I try to send address and size... still no answer.

 

Did somebody know why? What did I missed?

Outcomes