AnsweredAssumed Answered

STM3210E-EVAL USB operation

Question asked by holcomb.gregory on Aug 15, 2013
Latest reply on Aug 15, 2013 by Clive One
I'm working with the STM3210E demo board and trying to modify the USB Mass Storage demo function to access only the microSD memory and not the NVRam memory too.  I've removed reference to the NVRam such as initialization but when I connect up a USB cable its still coming up with two devices, two drive letters.  Can anybody point me to the area in that demo firmware that would need modification to tell the USB there is only one drive?

Outcomes