AnsweredAssumed Answered

STM32F103VET6 ,converts RGB/YCrCb image data to JPEG

Question asked by duong.tuan_anh on Aug 7, 2013
Latest reply on Aug 8, 2013 by Clive One
Can you help me a little bit?My thesis is about writing the code for image compression and decompression on STM32F103VET6. I have a RGB file and my tasks are writing 1 code to convert the RGB to a JPEG and writing 1 more code to compress the above JPEG into a smaller packet for transmission through  the 3G network using SIM5218.The receive side uses the STM32 hardware which can extract file into JPEG format.So, is it available if I only use the STM32? or any ic DSP else? Could you share the code for me if you have, please?My mail is: duongtuananh.hust @gmail.com. Thank you so much!

Outcomes