AnsweredAssumed Answered

Virtual COM Port CDC on STM32F4-Discovery

Question asked by fifre.pascal on Jul 29, 2013
Hi all,

I try to implement a CDC Device on STM32F4-discovery.
I made an IAR project based on the VCP example project of the STM32_USB-Host-Device_Lib_V2.1.0.

The STM32-Discovery starts correctly but two "STM32 Virtual ComPort in FS Mode" starts on my PC when I Plug the OTG connector on it.
When I analyze the USB frames on USB with USBlyzer, I see that two answer are returned on the getDescriptor.

Why do I have 2 answers on the getDescriptor?

Bets regards,

Pascal

Outcomes