AnsweredAssumed Answered

LSM9DS1 acceleration anti-aliasing filter

Question asked by Roussos.Giannis.001 on Jun 24, 2016
Latest reply on Jul 20, 2016 by Petr S
Hi all,
I have some questions regarding the LSM9DS1:
1. The Acceleration ODR choices go down to 10 Hz, however the bandwidth selection, presumable an anti-aliasing filter, is limited to 50Hz. Thus, when sampling at 10Hz or 50Hz with a bandwidth selection of 50Hz severe aliasing is to be expected. Is there a way to avoid this?
2. The accelerometed digital filter operation is not documented properly. What dow "high resolution" refer to? How is LPF or HPF selected?
3. Is there a block diagram for the acceleration signal available, similar to Figure 28 in the datasheet for the gyro signals?

Outcomes